Technical FAQs

Ask a Question

Is a HOM1632L200TCFT load center convertible to main breaker?

Issue:
Application

Product Line:
Homeline LC

Cause:
Convert MLO to MB

Resolution:
Yes, by removing the mainl lugs and field installing a QOM2-VH Main Breaker Kit, 200 ampere maximum. Catalog numbers available:
100 ampere - QOM2100VH
125 ampere - QOM2125VH
150 ampere - QOM2150VH
175 ampere - QOM2175VH
200 ampere - QOM2200VH


CTA-ID : 14023
Was this helpful?
What can we do to improve the information ?