Technical FAQs

Ask a Question

Did the old QO 'Wire-Gator' type load centers have copper bus, for example a QO130M150K?

Issue:
Old Design Product Features

Product Line:
QO Load Centers

Environment:
Bussing material

Cause:
Clarification of product features

Resolution:
The Old 'Wire-Gator' design, Convertible Mains QO Load centers had Tin Plated Copper Bus.
NOTE: ALL the old 'Wire-Gator' QO load centers are Obsolete and no longer available. BUT today Square D/SE offers a similar concept called "Qwik-Grip", see the FA318989 for catalog numbers.


 
Was this helpful?
What can we do to improve the information ?