Technical FAQs

Ask a Question

Is there a ground fault module for the Merlin Gerin Compact NSF UL listed circuit breaker?

No. However, there is a vigi ground fault module for the IEC version NS100/160/250.


CTA-ID : 14263
Was this helpful?
What can we do to improve the information ?