Technical FAQs

Ask a Question

What is the ambient operating temperature range for a HOMELINE load center? <br />

The normal ambient operating temperature range is -5 degree C (+23 degree F) to +40 degree C (+104 degree F), per NEMA Standards Publication PB-1, ``Panelboards``.


CTA-ID : 14262
Was this helpful?
What can we do to improve the information ?