Technical FAQs

Ask a Question

Is a QO12436L200TFT load center convertible to main breaker?

Issue:
Application

Product Line:
QO LC

Cause:
Convert MLO to MB

Resolution:
Yes, this Main Lugs Only load center can be converted to a Main Breaker load center by removing the factory installed main lugs and installing a QOM2 Main Breaker Kit, 200 ampere maximum. Catalog numbers for the Main Breaker Kits:
100 ampere - QOM2100VH
125 ampere - QOM2125VH
150 ampere - QOM2150VH
175 ampere - QOM2175VH
200 ampere - QOM2200VH


CTA-ID : 14011
Was this helpful?
What can we do to improve the information ?