Technical FAQs

Ask a Question

How do you determine which mounting plates to use on L140 cable pulls?

In Digest 172, pg. 19-25. The bottom of page indicates mounting plate styles; 1,2,3, or 4. This style is added to part number; ex; L143-2M would be - Style 2 mounting plate.

CTA-ID : 14005
Was this helpful?
What can we do to improve the information ?