Technical FAQs

Ask a Question

Can the 9001KA41 contacts be used with standard 3 position selector switches?

Yes, they can with the restriction that they can only be mounted on one side with all cams, except the B and L cams where they can be mounted on both sides.

CTA-ID : 13576
Was this helpful?
What can we do to improve the information ?