Technical FAQs

Ask a Question

In reference to a potentiometer operator, what is the difference between the the single pot and the tandem pot?

The tandem potentiometer has 2 pots, one mounted behind the other, on a single operator. The single potentiometer only has one pot mounted on the operator.

CTA-ID : 13571
Was this helpful?
What can we do to improve the information ?