Technical FAQs

Ask a Question

What are the repair parts for an HU363DSWA, Series E2 (may be shown as E02)?<br />

Issue:
old design repair parts

Product Line:
Heavy Duty Safety Switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:

The repair parts for the HU363DSWA, series E2 (E02) are as follows. No other parts are available.
-Line Base Assembly - 40512-560-50 (insulator, arc suppressor not included) LINE BASE IS NOW OBSOLETE, NLA WITH NO REPLACEMENT.
-Line Base Mounting Screw - 40205-065-01(3 required)
-Insulator - 40512-472-01
-Arc Suppressor Assembly - 40520-214-50 (includes mounting screws)
-Lug assembly - CL10F (includes 6 lugs)
-Lug Assembly Mounting Hardware - 23427-020-01
-Receptacle - WRDK1034
-Receptacle Mounting Screws - 45102-801-01 (required 4)
-Handle Knob Kit - 4028344050K (NOTE: this fits Series E Switches only)



CTA-ID : 14448
Was this helpful?
What can we do to improve the information ?