Technical FAQs

Ask a Question

Can the PDC6LA20 be used to feed a branch circuit?

No. This lug is not UL recognized for branch circuit application. It is for industrial control applications only. Switching to an M frame or using a power distribution block are the only options.


CTA-ID : 14238
Was this helpful?
What can we do to improve the information ?