Technical FAQs

Ask a Question

Do the XMLA/B pressure swtiches have unloader/bleeder valves on them?

No - unloader valves are not available on this product.
The 9013 types F and G have unloader valves available as an option on some products. If the range needed cannot be met by the these products, SQ D does not have anything else to offer. Telemecanique, however, does offer some options with metric fittings.


CTA-ID : 14231
Was this helpful?
What can we do to improve the information ?