Technical FAQs

Ask a Question

Do we offer a 9001 KM LED light module at 480 volts AC?

Issue:
Do we offer a 9001 KM LED light module at 480 volts AC?

Product Line:
Harmony Pushbuttons

Environment:
All Products

Cause:
Product Features

Resolution:
Use the 480 volt transformer light module and a 6 volt LED. Example: 9001 KM5LR will be a 480 volt AC transformer light module and a red LED. All the transformer light modules with LED`s are set up on the system, but they are not listed in the literature.


CTA-ID : 13535
Was this helpful?
What can we do to improve the information ?