Technical FAQs

Ask a Question

What are the repair parts for an H363DSWC, Series E1 (may be shown as E01)?

The repair parts for the H363DSWC, series E1 (E01) are as follows. No other parts are available.
-Line Base Assembly - 40512-558-50 (insulator, arc suppressor not included)
-Load Base Assembly - 40512-572-50
-Line and Load Base Mounting Screw - 40205-065-01(3 for line & 2 for load)
-Insulator - 40512-472-01
-Arc Suppressor Assembly - 40520-214-50 (includes mounting screws)
-Lug assembly - CL10F (includes 6 lugs)
-Lug Assembly Mounting Hardware - 23427-020-01
-Receptacle - 25410-022-95
-Receptacle Mounting Screws - 45102-801-01 (required 4)
-Handle Knob Kit - 4028344050K (NOTE: this fits Series E Switches only)

CTA-ID : 14443
Was this helpful?
What can we do to improve the information ?