Technical FAQs

Ask a Question

What is torque value for lugs on D325N?

Per the wiring diagram label on the inside of the switch, the main and neutral wiring binding screw should be torqued 340 inch pounds. Not foot pounds. Ground lug wire binding screw is 180 inch pounds.


CTA-ID : 14215
Was this helpful?
What can we do to improve the information ?