Technical FAQs

Ask a Question

What are the repair parts for an H362DSWA, Series E2 (may be shown as E02)?

Previous Design Repair Parts

Product Line:
Heavy Duty Safety Switches

Repair parts


The repair parts for the H362DSWA, series E2 (E02) are as follows. No other parts are available.
-Line Base Assembly - 40512-491-50 (insulator, arc suppressor not included)
-Load Base Assembly - 40512-500-50
-Line and Load Base Mounting Screw - 40205-065-01(3 for line & 2 for load)
-Insulator - 40520-114-01
-Arc Suppressor Assembly - 40512-399-50 (includes mounting screws)
-Lug Assembly - CL0306F (includes 6 lugs)
-Lug Assembly Mounting Hardware - 23425-017-00
-Receptacle - WRDK6034
-Receptacle Mounting Screws - 45102-801-01 (required 4)
-Handle Knob Kit - 4028344050K (NOTE: this fits Series E Switches only)

CTA-ID : 14440
Was this helpful?
What can we do to improve the information ?