Technical FAQs

Ask a Question

Can you add a phase to a DTU223NRB 2 pole device to make it a 3 phase device?

No.
1. The enclosure for the single phase will not be wide enough to accept another pole for 3 phase.
2. The label on the existing enclosure states that it is for use on single phase only.


CTA-ID : 14208
Was this helpful?
What can we do to improve the information ?