Technical FAQs

Ask a Question

What are the repair parts for the HU363AWA, series F4 (may be shown as F04)?

The repair parts for the HU363AWA, series F4 (F04) are as follows. No other parts are available.
-Line Base Assembly -40566-141-50 (requires one per switch. Arc suppressor assembly not included)
-Line Base Mounting Screw - 40205-151-01(3 required)
-Arc Suppressor Assembly - 40566-355-50 (requires one per switch)
-Arc Suppressor Mounting Screw - 40205-145-01
-Handle/Mechanism kit - HMR10FN12 (includes handle, mechanism, rod, and lockplate)
-Lug Kit - CL10F (one kit includes all line and load lugs)
-Receptacle - WRDK1034
-Receptacle Mounting Screws - 45102-801-01 (required 4)


CTA-ID : 14817
Was this helpful?
What can we do to improve the information ?