Technical FAQs

Ask a Question

Are optional lugs available for the AL800SN neutral assembly?

Yes, optional lugs are available for the AL800SN neutral assembly. The standard lug provided on the neutral assembly will accept (3) #3/0 AWG - 500 kcmil AL/CU conductors. Optional lugs include: AL800MA7 for (2) 500 - 750 kcmil AL/CU conductors: AL1000MA for (4) #1/0 AWG - 350 kcmil AL/CU conductors: CU1000MA for (3) #3/0 AWG - 500 kcmil CU only conductors. The optional lug kits contain one lug. Two kits would be required to change both the incoming and outgoing neutral lugs.
NOTE: The neutral assembly must be detached from its mounting pan to change out the lugs.

CTA-ID : 14427
Was this helpful?
What can we do to improve the information ?