Technical FAQs

Ask a Question

Does the QO130L200G load center have copper bus?

Issue:
Does the QO130L200G load center have copper bus?

Product Line:
QO and Homeline Load Centers

Environment:
Determining what material is used for the bus bars

Cause:
Meet specifications

Resolution:
Yes, this load center uses tin plated copper bus.



CTA-ID : 14617
Was this helpful?
What can we do to improve the information ?