Technical FAQs

Ask a Question

What is the clamping voltage for a 3 phase 120/208 v TVSS XGA type?

The UL suppression voltage raing on the XGA series is L-N (line to neutral) , L-G (line to ground), and N-G (neutral to ground) are 330 v and the L-L (line to line) is 700 v.
Refer to the Surge Protection Devices catalog section 6671CT9701R4/00, available on-line at www.squared.com, for technical information and product specifications.


CTA-ID : 14413
Was this helpful?
What can we do to improve the information ?