Technical FAQs

Ask a Question

9007C -- Y1903, 1905, 1901? Are these suffix numbers for a 5 or 4 pin connectors?

They are for a 5 pin Brad Harrison Connector # 41310 with #3 terminal as green ground pin. Different wire configurations will change the last digit. The prewired connector series begins with 190 and ends with a 2 digit configuration suffix. See the Help Files Forms list for more information.


CTA-ID : 14407
Was this helpful?
What can we do to improve the information ?