Technical FAQs

Ask a Question

Are the XMLE pressure switches suitable for use in a hazardous environment?

No, they are not rated for an explosive environment at all -and could not use an intrinsically safe relay to make it that way.
Digest 172, pg. 21-11.


CTA-ID : 14178
Was this helpful?
What can we do to improve the information ?