Technical FAQs

Ask a Question

Is the handle screw hole live to the on or off side of the PAF, PHF, PCF, PXF, PEF type breaker?

The handle screw hole and internal mechanism are live to both on and off side of the breaker.


CTA-ID : 14174
Was this helpful?
What can we do to improve the information ?