Technical FAQs

Ask a Question

How do you remove alternating function on the 9038 AG1.?

Customer must order either the form N3 or the form N4 on his 9038 AG1 in order to be able to remove the alternating function. N3 will provide a switch to select lead or lag. N4 will designate 1 as low level device and the second as the high level device.


CTA-ID : 14170
Was this helpful?
What can we do to improve the information ?