Technical FAQs

Ask a Question

9007 J How long is the standard Delrin extension?

The Delrin part is 2.85`` total length, .35`` goes into the spring, 2.5`` extends beyond the spring. The extensions (Digest 172, pg 19-5) do not extend the length, but are replacements.


CTA-ID : 13441
Was this helpful?
What can we do to improve the information ?