Technical FAQs

Ask a Question

Is the memory on the drives volatile or non-volatile?

The drive has non-volatile memory that is saved on EEPROM thus it is not lost when power is removed from drive nor keypad removed and should stay within the unit accordingly.


CTA-ID : 13207
Was this helpful?
What can we do to improve the information ?