Technical FAQs

Ask a Question

What considerations need to be taken into account when trying to select a drive for submersible pump application?

Need to first consider the full load amperage of motor that has been selected to size drive. (Assuming that torque requirements, etc. were taken into consideration when selecting motor). Would then need to take into cosideration length of output cable runs, possibility of capacitive coupling, subsequently possible need for use of inductors on output, consider use of check valves and whether pumping against pressure and possibility may need to go with constant torque drive versus variable torque.


CTA-ID : 13204
Was this helpful?
What can we do to improve the information ?