Technical FAQs

Ask a Question

How would you go about calculating the KVa size of transformer needed for a drive input when one is to be used?

To size the transformer and come up with the KVa would take the AC line current times AC line voltage times square root of 3 times 1.1

CTA-ID : 13203
Was this helpful?
What can we do to improve the information ?