Technical FAQs

Ask a Question

What are the repair parts for the H362A, series F3? (may be shown as F03)

Issue:
Previous Design Repair Parts

Product Line:
Heavy Duty Safety Switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:

The repair parts for the H362A, series F3 (F03) are as follows. No other parts are available.

Interior Kit - HSIF3606CF (includes line and load base Assemblies, mechanism, arc suppressor, all mtg. hardware and instructions).
Load Base Kit - HLB3606CF (includes load base, mtg. hardware and instructions)
Arc Suppressor Kit - HAS0610F (includes arc suppressor, mtg. hardware and instructions).
Lug Kit - CL0306F (includes 6-lugs and mtg. hardware)
Handle/Mechanism Kit - HM0610F (includes handle, mechanism, lockplate, gasket, all mtg. hardware and instructions).



CTA-ID : 13054
Was this helpful?
What can we do to improve the information ?