Technical FAQs

Ask a Question

Does Square D offer a 40 ampere version of the QOE250GFINM?

Issue:
Product design availability

Product Line:
QO load centers

Cause:
Application

Resolution:
No, Not as a factory assembled device. But one can use a QO24L60NRNM and field install a QO240GFI branch breaker.


CTA-ID : 12895
Was this helpful?
What can we do to improve the information ?