Technical FAQs

Ask a Question

What are the repair parts for a SC8L125F Series 002?

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only field replaceable parts.
Meter Cover kit - 40561-931-50
Load Center Cover kit - 40561-955-50
Utility lug cover kit (Pullbox) - 40561-930-50
Dead Front Cover kit - 40561-929-50
Meter socket (base) kit - 40561-933-50
Line side bus kit - 40561-934-50
Line side neutral kit - 40561-935-50
Load side neutral kit - 40561-959-50
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 13197
Was this helpful?
What can we do to improve the information ?