Technical FAQs

Ask a Question

What are the repair parts for a RC8L125C Series 002?

Issue:
Repair parts

Product Line:
CSED

Environment:
Repair parts

Cause:
Maintenance

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only field replaceable parts.
Rainproof Cap - 40561-158-03 (This is the top cap that covers the top endwall of the device)
Rainproof Cap Mounting Screws - (2) 21427-17161
Meter Cover kit - 40561-951-50
Load Center Cover kit - 40561-936-50
Utility lug cover kit (Pullbox) - same as meter cover kit
Dead Front Cover kit - 40561-929-50
Meter socket (base) kit - 40561-933-50
Ringless meter socket support brackets kit - 40561-952-50
Line side bus kit - 40561-934-50
Line side neutral kit - 40561-935-50
Load side neutral kit - 40561-959-50
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 13196
Was this helpful?
What can we do to improve the information ?