Technical FAQs

Ask a Question

What is the part number for the NEMA 3R HOMELINE load center interior trim mounting screw?

The 1/2`` long screw used to secure the interior trim is 4020513001K. This screw is a special triple lead, thread-forming screw that is only available through authorized Square D distributors.

CTA-ID : 13193
Was this helpful?
What can we do to improve the information ?