Technical FAQs

Ask a Question

What are the repair parts for the H322AWK, series F1? (may be shown as F01).

Issue:
Repair parts

Product Line:
HD SS

Cause:
Maintenance

Resolution:
The repair parts for the H322AWK, series F1 (F01) are as follows. No other parts are available.

Interior Kit - HSIF3603206CF (includes line & load base assemblies, arc suppressor, mechanism, fuse pullers, mounting hardware and instructions)
Load Base kit - HLB3603206CF (includes load base, mounting hardware and instructions)
Arc Suppressor kit - HAS0610F (includes arc suppressor, mounting hardware and instructions)
Lug kit - CL0306F (includes 6 Cu. lugs, mounting hardware and instructions)
Handle/Mechanism kit - HM0610F (includes handle, handle gasket, mechanism, lockplate, mounting hardware and instructions)
Handle Assembly - use handle/mechanism kit
Lockplate - use handle/mechanism kit
Fuse puller kit - FPK0610


CTA-ID : 13050
Was this helpful?
What can we do to improve the information ?