Technical FAQs

Ask a Question

What are the repair parts for the H322A, series F2? (may be shown as F02).

The repair parts for the H322A, series F2 (F02) are as follows. No other parts are available.

Interior Kit - HSIF3603206CF (includes line & load base assemblies, arc suppressor, mechanism, fuse pullers, mounting hardware and instructions)
Load Base kit - HLB3603206CF (includes load base, mounting hardware and instructions)
Arc Suppressor kit - HAS0610F (includes arc suppressor, mounting hardware and instructions)
Lug kit - CL0306F (includes 6 Cu. lugs, mounting hardware and instructions)
Handle/Mechanism kit - HM0610F (includes handle, handle gasket, mechanism, lockplate, mounting hardware and instructions)
Handle Assembly - use handle/mechanism kit
Lockplate - use handle/mechanism kit
Fuse puller kit - FPK0610


CTA-ID : 13048
Was this helpful?
What can we do to improve the information ?