Technical FAQs

Ask a Question

What plug is required for use with the receptacle used on a H362WA, H362DSWA, H362CSWA and H362AWA (safety switch with Appleton POWERTITE receptacle installed)?

Issue:
Selection

Product Line:
HD SS

Cause:
Accessory Selection

Resolution:
The receptacle is UL Listed for use with Square D or Appleton plug # ACP6034BC. It is also UL Classified for use with Square D or Crouse-Hinds ARKTITE plug # APJ6485.



CTA-ID : 12879
Was this helpful?
What can we do to improve the information ?