Technical FAQs

Ask a Question

What plug is required for use with the receptacle used on a HU361WA, HU361DSWA, HU361CSWA and HU361AWA (safety switch with Appleton POWERTITE receptacle installed)?

Issue:
Selection

Product Line:
HD SS

Cause:
Accessory Selection

Resolution:
The receptacle is UL Listed for use with Square D or Appleton plug # ACP3034BC. It is also UL Classified for use with Square D or Crouse-Hinds ARKTITE plug # APJ3485.



CTA-ID : 12878
Was this helpful?
What can we do to improve the information ?