Technical FAQs

Ask a Question

Is the SDSB1175C suitable for use in Category B or Category C locations?

Yes, it is suitable for use in Category B and C locations.
ANSI/IEEE C62.41-1991 Location Categories are defined as:
C - Outside and service entrance
Service drop from pole to building
Run between meter and panel
Overhead line to detached building
B - Feeders and short branch circuits
Distribution panel devices
Heavy appliance outlets with short connections to service entrance
A - Outlets and long branch circuits (All outlets at more than 30` (10m) from Category B) (All outlets at more than 60` (20m) from Category C)

CTA-ID : 13188
Was this helpful?
What can we do to improve the information ?