Technical FAQs

Ask a Question

Can multiple motor leads fed from AC Drives share a conduit or raceway?

It is not recommended that output cables from different AC drives share close proximity in raceways or conduits. Because of the high frequency switching and increased capacitance, the drive may fault under some conditions. Damage to the drive and/or motor may result from disregarding this recommendation.

For example, see page 39 of the manual VD0C06S304E. Similar wording is found in many other publications

CTA-ID : 13180
Was this helpful?
What can we do to improve the information ?