Technical FAQs

Ask a Question

What are the repair parts for the H222AWK, series F4? (may be shown as F04)

Issue:
Repair parts

Product Line:
HD SS

Cause:
Maintenance

Resolution:
The repair parts for the H222AWK, series F4 (F04) are as follows. No other parts are available.

Line Base Assembly - 40566-425-50 (arc suppressor not included)
Load Base Assembly - 40566-361-50
Arc Suppressor Assembly - HAS0610F
Lug Assembly - CL0306F (includes 6 lugs)
Mechanism Assembly - 40566-107-50
Handle Assembly - 4056684150K
Handle Gasket - 40566-031-01
Lockplate - 40566-376-01
Line & Load Base mounting screw - 40205-160-01 (3 for line & 2 for load)
Arc Suppressor mounting screw - 40205-145-01 (1 required)
Lockplate mounting screw - 22999-405-62 (2 required)


CTA-ID : 13040
Was this helpful?
What can we do to improve the information ?