Technical FAQs

Ask a Question

What are the repair parts for the H222A, series F4? (may be shown as F04)

The repair parts for the H222A, series F4 (F04) are as follows. No other parts are available.

Line Base Assembly - 40566-425-50 (arc suppressor not included)
Load Base Assembly - 40566-361-50
Arc Suppressor Assembly - 40560-018-01
Lug Assembly - CL0306F (includes 6 lugs)
Mechanism Assembly - 40566-107-50
Handle Assembly - 4056684150K
Handle Gasket - 40566-031-01
Lockplate - 40566-376-01
Line & Load Base mounting screw - 40205-160-01 (3 for line & 2 for load)
Arc Suppressor mounting screw - 40205-145-01 (1 required)
Lockplate mounting screw - 22999-405-62 (2 required)


CTA-ID : 13039
Was this helpful?
What can we do to improve the information ?