Technical FAQs

Ask a Question

Are any of the Type L limit or emergency stop cable pulls explosion proof rated?

No none of the type L cable pull devices or limit switch are explosion proof.

Alternate look at the 9007 Type CR in Digest 172 page 19-4.

CTA-ID : 12877
Was this helpful?
What can we do to improve the information ?