Technical FAQs

Ask a Question

Is 9007CR53J rod suitable for contact with kerosene?

J rod is Delrin, an acetyl resin which should withstand gasoline and many solvents. Customer must make determination if this is an appropriate material for their use.


CTA-ID : 13404
Was this helpful?
What can we do to improve the information ?