Technical FAQs

Ask a Question

Why do you not recommend running a motor above base speed higher than 62hz in variable torque mode?

The motor manufacturer needs to be contacted to confirm operation of motor above base speed to ensure it can be handled and thus we can not guarantee its operation. Additionaly, you need to be aware that in variable torque application above base speed the current becomes square of itself as speed increases.

CTA-ID : 13178
Was this helpful?
What can we do to improve the information ?