Technical FAQs

Ask a Question

What are the repair parts for the HU462 series F03? (may be shown as F03)

Repair parts

Product Line:
Heavy Duty Safety Switch


The repair parts for the HU462, series F3 (F03) are as follows. No other parts are available.

Interior kit - HSIU4603606F (Includes line base assembly, mechanism, arc suppressor, all mounting hardware and instructions).
Arc Suppressor kit - HAS0610F - (TWO required, includes arc suppressor & mounting hardware)
Lug kit - AL0306F - (TWO required, kit includes 6 lugs)
Handle/Mechanism kit- HM0610F(kit includes handle, mechanism, lockplate & mounting hardware)

CTA-ID : 13037
Was this helpful?
What can we do to improve the information ?