Technical FAQs

Ask a Question

What are the repair parts for the H462, series F3? (may be shown as F03).

Issue:
Repair Parts

Product Line:
Heavy Duty Safety Switch

Cause:
Maintenance

Resolution:
The repair parts for the H462, series F3 (F03) are as follows. No other parts are available.

Interior Kit - HSIF4606F (includes line & load base assemblies, arc suppressor, mechanism, mounting hardware and instructions)
Load Base kit - HLB2606F (2-required, includes load base, mounting hardware and instructions)
Arc Suppressor kit - HAS0610F (2-required, includes arc suppressor, mounting hardware and instructions)
Lug kit - AL0306F (2-required, includes 6 lugs, mounting hardware and instructions)
Handle/Mechanism kit - HM0610F (includes handle, handle gasket, mechanism, lockplate, mounting hardware and instructions)
Handle Assembly - use handle/mechanism kit
Lockplate - use handle/mechanism kit


CTA-ID : 13030
Was this helpful?
What can we do to improve the information ?