Technical FAQs

Ask a Question

9007R20 Customer is asking for the amount of adjustment.<br /><br />

This is a roller that slides on a rod supplied by the customer. That rod, attached to a 9007R16 or R17, can be any length that the customer chooses.

CTA-ID : 12861
Was this helpful?
What can we do to improve the information ?