Technical FAQs

Ask a Question

What is the wire range of the lugs used in a MPR33125?

The line phase and neutral lugs accept (1) #1/0 AWG - 600 kcmil or (2) #1/0 AWG - 250 kcmil Al/Cu conductors.


CTA-ID : 13363
Was this helpful?
What can we do to improve the information ?