Technical FAQs

Ask a Question

What is the standard rating of the line reactor used in the Econo-Flex units and ATV58 drives when provided standardly because need to meet a IEEE specification?

The line reactor rating is less than 3% but unit does still meet IEEE standard when properly applied to system.


CTA-ID : 13165
Was this helpful?
What can we do to improve the information ?