Technical FAQs

Ask a Question

Can a circuit breaker be used instead of line fuses on the drives?

Square D does not recommend replacing line fuses were specified by using any other short circuit protection because what is recommended constitutes what the North American market has tested and is UL approved. Fuses are also recommended because they are tested to open quicker than circuit breakers, etc. according to their various ratings.

CTA-ID : 13164
Was this helpful?
What can we do to improve the information ?